Press Release
<< Back
Generac Power Systems Launches HomeLink Upgradeable Manual Transfer Switch
With one push of a button, this versatile, innovative transfer switch allows homeowners to easily harness the power of their portable generator to power hard-wired circuits in their home. And when homeowners decide to upgrade to an automatic home backup generator, HomeLink is designed so electricians can simply change out the subpanel, conveniently preparing the prewired switch for an automatic home generator to back up essential circuits (max 11 kW). This saves homeowners money because all the circuits have already been wired.
"This is a great product for homeowners because it provides an affordable and safe solution for backup power with a portable generator," said
As with other
Customers can choose from three different models. All include eight circuits, but can hold a maximum of 10. Each switch comes standard with a five-year, limited warranty.
HomeLink is available through all participating
About
Since 1959,
Logo - http://photos.prnewswire.com/prnh/20140304/CG76575LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/generac-power-systems-launches-homelink-upgradeable-manual-transfer-switch-300030284.html
SOURCE
Heather Gaedtke, Cramer-Krasselt Public Relations, 414-227-3505, hgaedtke@c-k.com; or Rachel Tracey, Generac Marketing Communications, 262-544-4811 ext. 2648, Rachel.Tracey@generac.com