Press Release
<< Back
Mean Green Launches FURY, New Compact Electric Mower
One of the narrowest battery-powered, stand-on mowers available in market
"We're excited to expand our line of commercial-grade mowing solutions and give landscape professionals a perfect option to complete their fleets with the FURY," said
The FURY joins Mean Green's full-sized mower the VANQUISH (52- or 60-inch mowing width), to complete the line of commercial, electric-powered, stand-on mowers that can run all day on a single charge. The FURY is available with either a side- or rear-discharge mulching deck and uses the same patented zero-turn technologies found in all Mean Green mowers.
The FURY features an 11kWh fixed battery (24 HP equivalent) that runs for up to 7 hours on a single charge at speeds up to 9mph, and recharges in as little as 5 hours. A 5-year or 1500-hour commercial battery warranty is standard with purchase.
About Mean Green
Mean Green, founded in 2009, designs and manufacturers an innovative commercial line of zero-turn and walk behind, battery powered turf care products that provide quiet operation, zero emissions and minimal maintenance options as compared to traditional commercial mowers. Mean Green commercial-grade mowers are designed to run continuously for up to 8 hours on a single charge using patented technology and lithium battery power. Mean Green proudly manufactures in the towns of
About
Media Contact: Stephanie Rodgers
Stephanie.Rodgers@Generac.com
Phone: 262.544.4811 Ext. 4456
View original content to download multimedia:https://www.prnewswire.com/news-releases/mean-green-launches-fury-new-compact-electric-mower-301752067.html
SOURCE Mean Green