Press Release
<< Back
Generac Introduces PWRmanager for Whole Home Power
PWRmanager allows homeowners to use their phone or tablet to simply "swipe" off/on any circuit in their home. This can extend battery runtime during prolonged power outages by de-energizing less important circuits. And for homeowners who want to run their homes on stored sunshine on a daily basis, PWRmanager is designed to provide an uncompromised experience that other solar and battery systems simply cannot.
"The Generac PWRcell System is the most powerful battery system on the market, and now with PWRmanager, we've taken it a step further," said
PWRmanager is designed as an easy-to-install device and does not require a new load panel. Rather, it installs next to the home's existing electrical panel in as little as 90 minutes. Additionally, the PWRmanager is priced lower than other similar products and integrates seamlessly with the PWRcell System and PWRview app. PWRmanager automates control of up to twelve 120V circuits or six 240V circuits, plus two thermostats.
"In a power outage, every bit of battery power is important," Minick said. "PWRmanager makes choices about how and when appliances get power on your behalf, so that you have the best outage experience possible and do not have to compromise on comfort or lifestyle."
PWRmanager will be available for purchase beginning in Spring 2022. For more information about PWRmanager or other
About
Contact: |
|
262-544-4811 Ext. 3950 |
View original content to download multimedia:https://www.prnewswire.com/news-releases/generac-introduces-pwrmanager-for-whole-home-power-301381692.html
SOURCE