Press Release
<< Back
Back-to-Back Nor'easters Prove Power Outage Preparedness Tops Homeowners' Priorities
While many are still trying to clean up from the previous storm, homeowners can prevent further damage and loss before the next storm arrives by purchasing an emergency generator. Here are some tips to choose the option that is the best fit for the homeowner's needs:
Portable Generators:
A portable generator can be a good option for those who are looking to power the most critical home items. They are simple to buy, easy to run and can power most essential lights or appliances via extension cords. Portable generators must be placed outside, far away from windows and doors and in a dry place.
Manual Transfer Switches:
A manual transfer switch can be used in combination with a portable generator to allow people to backup more items in their homes -- even hard-wired appliances like a furnace or well pump -- by delivering emergency power through the home's electrical system. There's no need to run extension cords from the generator to the lights and appliances. It is wired directly to the home's electrical panel and can power circuits of the homeowner's choosing. A manual transfer switch is the only safe way to deliver power from a portable generator to the home's electrical system, and while you will not likely be able to have one installed before Quinn, you can work with an authorized
Home Standby Generator:
While it's not possible to install a standby home generator ahead of this storm, there are certain to be future power outages. A home standby generator is a permanently installed solution and is connected to the home's existing natural gas or propane line. It sits outside the home, much like an air conditioning unit. These generators can restore power to the home -- units are even available that can back up the entire home -- within seconds of an outage. One of the more than 5,000
Just because the storm ends doesn't mean the threat does. The failing U.S. infrastructure makes access to power vulnerable in severe weather. Homeowners can take control and power their own home with the help of a
About
Media Contacts
View original content with multimedia:http://www.prnewswire.com/news-releases/back-to-back-noreasters-prove-power-outage-preparedness-tops-homeowners-priorities-300610040.html
SOURCE