Investor Relations

Press Release

View printer-friendly version

<<  Back

A New Outdoor Power Equipment Line for Commercial and Rental Use

Generac Pro line engineered and designed specifically for professionals

WAUKESHA, Wis., Feb. 6, 2018 /PRNewswire/ -- At The Rental Show 2018, Generac® will be introducing attendees to its new Generac Pro line of rugged outdoor power equipment designed and engineered specifically for commercial users, such as landscape contractors, and rental applications. The new assortment, under the Generac Pro brand, will consist of the following products (hi-res images are available for download at http://bit.ly/GeneracProImages):  

  • XC Series portable generators (6500 and 8000 watts)
  • XD5000E diesel-fueled portable generator
  • 3800 PSI belt drive pressure washer (3.2 gpm)
  • Walk-behind field and brush mowers with 26-in. and 30-in. cut
  • Tow-behind field and brush mower with a 44-in. deck
  • Walk-behind trimmer with a 22-in. cutting width
  • 60-in. power grader
  • 34-ton hydraulic wood splitter with a road tow kit
  • Chipper/shredder with a road tow kit
  • Stump grinder
  • Trash and semi-trash water pumps
  • Towable backhoe with a 12-in. bucket
  • Powerwagon with an 8.0-cu.ft. bucket and 800-lb. hauling capacity

Many of the products under the Generac Pro banner are powered by the company's G-Force engine, originally designed by Generac specifically for generator applications and first introduced on the company's XC Series portable generators.

"The many retailers, contractors and rental companies we've spoken with in developing the Generac Pro line have told us they want a high-quality, high-value alternative to Honda-powered products," Gatzke said. "We believe powering the Generac Pro line with Generac G-Force engines meets that need."

The Generac Pro line will be supported by Generac's nationwide network of parts and service providers. "Our network guarantees same-day shipping on all service parts and 48-hour delivery," Gatzke said. "That means downtime is minimized on the job site."

Generac Pro products will be highlighted at the company's booth 6727 at The Rental Show. Media interested in attending an event on Tuesday, Feb. 20 at 9:30am in the booth in which product experts will present and demonstrate these and other products should contact Art Aiello, public relations manager, for more details at art.aiello@generac.com or 262-544-4811, ext. 2987.

About Generac

Generac Power Systems, Inc. (NYSE: GNRC) is a leading global supplier of backup power and prime power products, systems and engine-powered tools. Back in 1959, our founder was committed to designing, engineering and manufacturing the first affordable backup generator. Fifty-seven years later, the same dedication to innovation, durability and excellence has resulted in the company's ability to expand its industry-leading product portfolio into homes and small businesses, on job sites, and in industrial and mobile applications across the globe. Generac offers single engine backup and prime power systems up to 2 MW and paralleled solutions up to 100 MW, and uses a variety of fuel sources to support power needs for our customers. We are proud to be named, in back-to-back years, the Frost & Sullivan 2014 and 2015 North American Natural Gas Generator Set Company of the Year. Visit Generac.com for more information.

Media Contacts
Art Aiello | Generac Public Relations | 262-544-4811 x 2987 | art.aiello@generac.com

The Generac Pro line of outdoor power equipment has been engineered and designed specifically for commercial users, such as landscape contractors, and rental applications.

 

Cision View original content with multimedia:http://www.prnewswire.com/news-releases/a-new-outdoor-power-equipment-line-for-commercial-and-rental-use-300594530.html

SOURCE Generac Power Systems, Inc.