Press Release
<< Back
Most Americans Choose TV Over Heat
Severe winter storms are often times accompanied by extended power outages that can be life-threatening in sub zero temperatures. But a new study from
"The study results prove that many Americans think more about the inconvenience of a power outage than the life threatening affects a long term outage can have during the cold winter months," said
In addition to power outages, there are several dangers associated with winter storms, including damage from the weight of ice, snow and sleet. In the cases of major snowstorms, homeowners can even be trapped in their homes due to blocked or frozen entryways. Cracked or burst water pipes connected to anything from steam and hot water heating or a fire-protection system can be extremely costly. Even after the storm, melting snow can cause major flooding.
"Though the list of winter weather dangers runs long,
- Install weather stripping.
- Have your furnace/heating system serviced at the beginning of each season to ensure it runs properly, and have the filters changed.
- Move furniture away from vents.
- Add rock salt and sand to emergency kits to help melt ice on walkways.
- Install roof-heating cables to prevent ice dams on roofs and gutters.
- Insulate pipes and winterize your sprinkler system by turning off the water supply and ridding the pipes of excess water by blowing compressed air through the sprinkler lines.
- Run the water regularly to help prevent pipes from freezing and bursting. Opening the faucet, even just a drip, will provide relief from the excessive pressure that comes with ice blockage and can prevent a burst pipe.
- Insulate outlets with gasket covers.
- Install attic insulation, which can save as much as 30 percent on heating costs. It's also suggested to place a cover over attic stairs.
- Invest in an automatic home standby generator, like those from
Generac , that automatically provide power for heat and electricity when there is a power outage. Automatic home backup generators turn on automatically as soon as the power goes out and stay on until utility power is restored.
Just 29% of Americans surveyed own a source of backup power, meaning the majority of homeowners could face life threatening danger if an outage hit their area.
"The study demonstrates that the majority of Americans don't take winter storms, and potential outages, seriously. Winterizing your home is a lot easier than most homeowners think," said Feng. "Because it is so easy to do, homeowners should really make it a priority each year to keep their homes and families safe. And the best time to prepare is now, before the snowflakes start to fly."
If you are interested in additional information about how to properly prepare your home for winter,
Additional information on winter weather preparedness is available at http://www.ready.gov/winter-weather and http://www.generac.com/stormprep. Consumers can also log on to www.generac.com and click on the dealer locater to find a local dealer and sign up for a free in home assessment.
About
Logo - http://photos.prnewswire.com/prnh/20140304/CG76575LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/most-americans-choose-tv-over-heat-300177742.html
SOURCE
Heather Gaedtke, Cramer-Krasselt Public Relations, 414-227-3505, hgaedtke@c-k.com; Hannah Thulin, Cramer-Krasselt Public Relations, 414-227-3530, hthulin@c-k.com