Press Release
<< Back
Hurricane Joaquin Expected to Intensify; East Coast Has Minimal Time to Prepare
"Hurricanes are unpredictable, so it's especially important for residents in areas that are in the projected path of the storm to prepare as early as possible," said
While many forecasters expect Joaquin to intensify and make landfall along the
For those not sure where to start,
- Charge your electronics: Like storms, the power outages associated with them are very unpredictable. Our homes and lifestyles today are more reliant on technology than ever, so charge your cell phone, computer and other electronic devices before the storm hits. Put new batteries in flashlights and have a backup case of batteries in a watertight container.
- Remove outdoor furniture and loose foliage: Hurricane winds can reach 100 miles per hour or more depending on the storm's category. Outdoor furniture or loose foliage can become a projectile, causing damage to your home or nearby buildings. Bring them inside to eliminate the risk.
- Stock up on essentials: Having gallons of water, a storage room with food, extra batteries and waterproof emergency numbers on hand is a smart idea on its own, but will come in extra handy if you can't leave your home during a hurricane.
- Choose a backup power source: Generators can be lifesaving when severe weather causes an outage. From keeping refrigerated medicine cold to powering lights or a cell phone charger, generators are an important lifeline to keep families and homes safe and protected. Both portable and home standby generators offer benefits, and residents of all kinds are encouraged to include this technology as part of their preparedness plans.
It is also important to remind portable generator users of proper safety procedures to ensure their family's continued safety while using their generator.
- NEVER run a generator indoors or in partly enclosed areas such as garages.
- Do not overfill the fuel tank. Always allow room for fuel expansion.
- Do not smoke near fuel or generator.
- Connecting a portable electric generator directly to your household wiring can be deadly to you and others. Home standby generators are a better option if you're looking for something to connect directly to household wiring.
- Only start or stop the generator when no electrical loads are connected.
- Overloading your generator can seriously damage your valuable appliances and electronics.
- The generator must be properly grounded. If the generator is not grounded, you run the risk of electrocution.
- Keep children away from portable generators at all times.
- Allow at least 5 feet of clearance on all sides of the generator when operating.
Preparing your family now, before the storm hits, is the best way to prevent damage, power outages and stress during Hurricane Joaquin.
Learn More
For more facts and advice, visit www.Generac.com/be-prepared or call 888-
About
Since 1959,
Logo - http://photos.prnewswire.com/prnh/20140304/CG76575LOGO
To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/hurricane-joaquin-expected-to-intensify-east-coast-has-minimal-time-to-prepare-300152741.html
SOURCE
Heather Shannon Gaedtke, Cramer-Krasselt Public Relations, 414-227-3505, hgaedtke@c-k.com; or Jodi Marose, Generac Public Relations Manager, 262-544-4811 x2771, Jodi.Marose@generac.com