Press Release
<< Back
Good Design Awards Honors Multiple Products from Generac
Awards for five products across the portfolio reflect the company's dedication to innovative design
Celebrating its 73rd anniversary, the GOOD DESIGN Awards program is one of the oldest design competitions in the world. Every year, the program selects a list of product designs and graphics that have chartered new directions for innovation and pushed the envelope for competitive products in the world marketplace.
"It is an honor to be recognized by the GOOD DESIGN Awards. We strive to create designs that are highly functional for customers and also progressive in their impact and relevance for a better future," said
GB1000 and GB2000
The Generac GB1000 and GB2000 Portable Power Stations provide the advantages of clean, emission-free AC or DC power output at the push of a button. With its ergonomic handle and compact, durable, and lightweight enclosure, the Portable Power Station is built for power to be taken and used virtually anywhere – indoors or outdoors. The GB1000 (1086kWh capacity) and GB2000 (2106kWh capacity) models can power a wide range of electronics, such as phones, refrigerators, sump pumps, laptops, power tools and more. The units provide convenient power access with integrated AC and 12V DC outlets, USB ports and a 15W wireless charging pad. Both models also feature a large, 4.7" multi-color display that shows key data, including charge level, run-time, and current output.
The Generac MLTB, or
DR Power Equipment ZT5e
The DR Power Equipment ZT5e Zero-Turn battery-powered mower allows for virtually maintenance-free lawn care. With a full charge, you can mow for up to 1.75 hours utilizing a 60" mowing width to mow as much as five acres. Recharge overnight and you're ready to go again the next day, DR's unique battery packs are designed to function either independently or as a set that can be drawn on, or charged, as an interconnected array. Use one, two, or three batteries in the ZT5e: each is 2.5 kWh, allowing for up to 7.5 kWh to maximize run time.
PWRmanager
The Generac PWRmanager was designed with an understanding of the challenges in power management as well as everyday user needs. With the growing demand for efficient energy utilization, the product provides real-time monitoring, customizable settings, and seamless integration with the Generac PWRview app. This empowers users to track and control their power usage, enables making informed decisions, reduces costs, and contributes to a more sustainable future. This user-centric approach makes PWRmanager an indispensable tool for individuals and businesses seeking to optimize their power consumption and enhance overall energy management.
For more information about the GOOD DESIGN Awards, please visit the official website: https://www.good-designawards.com/
About
Media Contact: Stephanie Rodgers
Stephanie.Rodgers@Generac.com | (262) 968-8252
View original content to download multimedia:https://www.prnewswire.com/news-releases/good-design-awards-honors-multiple-products-from-generac-302052408.html
SOURCE