Press Release
<< Back
Generac Urges Planning Ahead for Power Outages During National Preparedness Month
Rising number of severe weather events driving need for power outage plans
The growing impact of extreme weather has resulted in
"National Preparedness Month is exceptionally critical this year, as we will continue seeing increased severe weather activity result in power outages," said
During National Preparedness Month,
- Portable Open Frame Generators can sustain a home continually during an outage and don't require recharging, as they're powered by gas, diesel or liquid propane. This option can support large household demands and can run for more than ten hours at 50% load, helping homeowners stay safe and comfortable when the power goes out. Portable generators must be run outdoors and far away from doors, windows, and vents to avoid carbon monoxide poisoning. Regular maintenance and monitoring of the oil and air filters will keep a portable generator ready for the next emergency.
- Inverter Generators are more compact and efficient than classic portable generators, offering the ability to power up or down depending on demand. Durable and lightweight, inverters can be picked up and carried, making them a versatile option for providing power at home or work. Inverters feature an easy start function, with no need to pull a cord, and can provide over eight hours of power at 50% load. Inverter Generators also offer a Total Harmonic Distortion below 5%, making them generally suitable for a variety of sensitive electronics, tools, and appliances. Like other portable generators, inverters must be operated outside and far away from doors, windows, and vents for safety.
- Battery-Powered Portable Power Stations are quiet, emission-free, and the easiest to transport due to their small size. Portable power stations don't require fuel, and they offer the opportunity for indoor use, such as in apartments or condos. They can recharge from 0-80% in as little as two hours from a standard wall outlet, but also have the versatile ability to recharge through car, generator, or portable solar panels (available separately).
- Home Standby Generators are permanently installed outside the home and automatically kick in during a power outage, delivering seamless power to the whole home. They offer convenience, comfort, and confidence, ensuring the ability to maintain typical lifestyle patterns during an outage.
In addition to early preparation, homeowners and business owners should stay informed of local power outages.
For more tips to help plan for power outages and information on home backup power solutions, visit www.generac.com/beprepared.
About Generac
Media Contact:
Stephanie.Rodgers@Generac.com
Phone: 262.544.4811 Ext. 4456
View original content to download multimedia:https://www.prnewswire.com/news-releases/generac-urges-planning-ahead-for-power-outages-during-national-preparedness-month-301924664.html
SOURCE