Press Release
<< Back
Generac Unveils Next Generation PWRcell Energy Storage Products at RE+
New products offer smarter, more powerful and resilient solutions to enable more choice and control in the way people use sustainable energy sources
PWRcell 2 delivers 18 kWh capacity in a single cabinet and 10 kW max continuous power, enough power to start virtually any single load in the home during an outage, including a 5-ton A/C unit. PWRcell 2 MAX will feature even more power at launch, with 11.5 kW max continuous power. It will also have the capability to start loads greater than 200A LRA, higher efficiency and a broader operating temperature range.
Both products are designed to integrate seamlessly with Generac's family of generator products, giving customers a smart, open ecosystem for greater resiliency and energy independence. In the event of a multi-day power outage, customers will have peace of mind with a paired PWRcell 2 and Generac brand generator*. If the PWRcell 2 battery reserves are low, the generator can power the home and recharge the battery simultaneously, keeping families comfortable during extended outages.
PWRcell 2 and PWRcell 2 MAX enable seamless home energy management and feature native integration with ecobee smart thermostats* providing an in-home display where homeowners can monitor their storage system, helping them save on energy bills.
When paired with PWRcell 2 or PWRcell 2 MAX, the ecobee smart thermostat provides alert notifications and automatically adjusts temperature set points during outages, preserving stored energy and extending backup duration. PWRcell 2 will be available by the end of the year and PWRcell 2 MAX will debut in the second half of 2025.
"With rising energy costs and increasingly frequent power outages, home energy management is critical for our customers. With PWRcell 2 and PWRcell 2 MAX, we are enabling smarter, powered homes that deliver reliability and resilience while providing customers the ability to quickly respond to their changing energy needs," said
PWRcell 2 and PWRcell 2 MAX are eligible for financing to qualifying customers through Mosaic and Palmetto's Lightreach financial products and will be made available on all the existing Lightreach integrated 3rd party platforms at launch, with several more financing platforms to follow.
*Sold separately
About
Generac Holdings (NYSE:GNRC) is a leading energy technology company that provides backup and prime power products and energy storage systems for home and business applications, as well as energy monitoring and management devices and services, along with other power products. Founded in 1959,
Media Contact:
Jonathan.Stern@Generac.com | (312) 402-7167
View original content to download multimedia:https://www.prnewswire.com/news-releases/generac-unveils-next-generation-pwrcell-energy-storage-products-at-re-302242965.html
SOURCE