Investor Relations

Press Release

View printer-friendly version

<<  Back

Generac Power Systems Introduces Innovative PowerDial™ Control Pressure Washer

The exclusive PowerDial feature simplifies residential cleaning tasks, putting the user in complete control

WAUKESHA, Wis., July 28, 2015 /PRNewswire/ -- Generac Power Systems, a leading designer and manufacturer of backup power generators and engine-powered tools, is pleased to introduce its new residential 2000-3000PSI Variable Pressure Washer. The unit features Generac's innovative PowerDial, which allows users to easily control pressure settings, enhancing usability and providing the necessary versatility to clean a variety of surfaces without having to use multiple units.

Generac is a leading manufacturer of generators and provides a broad range of power solutions.

Generac's unique PowerDial has four adjustable settings that allow users to clean virtually any surface – from cars and boats, to brick and concrete. Users can easily turn the PowerDial to select the appropriate PSI for their cleaning job – no matter how tough or delicate. In a matter of seconds, owners can go from cleaning a car at 2000PSI to blasting dirt and grime off concrete at 3000PSI.

"We designed this pressure washer with the goal of delivering more versatility and usability than other pressure washers in the market," said David Lincoln, senior product manager for Generac Power Systems. "It's affordable and a great tool to have on hand to get outside cleaning jobs done fast."

Generac applied many features to the Variable Pressure Washer that have proven popular on its other pressure washers. For example, the spray gun features a soft grip for comfort, and an easy-to-pull inverted trigger design that requires minimum effort; both reduce fatigue during prolonged use. Additionally, the Generac overhead valve (OHV) horizontal-shaft engine makes the pump more accessible by positioning it well above the ground so users can easily make hose connections, and the fuel tank is up to three-times larger than most competitive units. 

Other notable features include:

  • CARB compliant engine, approved for sale in California
  • Equipped with never-flat wheels for ease of transportation
  • 25-foot non-marring high pressure hose to avoid kinks and damage
  • Folding frame for easy transport and storage

The 2000-3000PSI Variable Pressure Washer is available at participating retailers and dealers for just $399. Click here to find the nearest dealer or retailer, or visit www.Generac.com for more information.

About Generac (NYSE: GNRC)
Generac Power Systems (NYSE: GNRC) is a leading global supplier of backup power and prime power products, systems, and engine-powered tools. Back in 1959, our founder was committed to designing, engineering, and manufacturing the first affordable backup generator. Fifty-five years later, the same dedication to innovation, durability and excellence has resulted in the company's ability to expand its industry-leading product portfolio into homes and small businesses, on job sites, and in industrial and mobile applications across the globe. Generac offers backup and prime power systems up to 100 MW, and uses a variety of fuel sources to support power needs for our customers. We are proud to be named the Frost & Sullivan 2014 North American Natural Gas Generator Set Company of the Year.

Logo - http://photos.prnewswire.com/prnh/20140304/CG76575LOGO

 

To view the original version on PR Newswire, visit:http://www.prnewswire.com/news-releases/generac-power-systems-introduces-innovative-powerdial-control-pressure-washer-300120024.html

SOURCE Generac Power Systems

Heather Gaedtke, Cramer-Krasselt Public Relations, 414-227-3505, hgaedtke@c-k.com; or Rachel Tracey, Generac Marketing Communications, 262-544-4811 ext. 2648, Rachel.Tracey@generac.com