Press Release
<< Back
Five Ways a Power Outage Can Cost You Money
Extended power outages can impact your checkbook in many ways:
- Lost refrigerated and frozen goods. The USDA recommends throwing away refrigerated foods stored for more than two hours at over 40 degrees Fahrenheit, because refrigerators and freezers can't stay cold without electricity. For a family with a full-stocked freezer and fridge, that means a loss of at least
$200 in tossed food. - Damage to your home. Without power, sump pumps can't run, putting homes at risk for flooding, and fans and dehumidifiers can't operate to help dry out a wet basement. A power outage during a severe storm can destroy basements and pose significant hazards to homeowners. Basic costs to pump out and thoroughly dry a basement lightly flooded with clean water can start between
$500-$1,500 and increase to$2,000-$10,000 . But a flooded basement can be prevented, even during the most severe storms, with a home backup generator. - Expenses from staying at a hotel or eating out. If you don't have heat or running water, you might have to move the family into a hotel for a night or two. Add restaurant tabs to that and you've lost another couple hundred dollars.
- Additional costs for short-term goods. If you choose to remain in your home, you will need to invest in batteries for radios and flashlights, coolers to store food, and ice to keep that food cold. Incidental costs can range from $200 to $500.
- Loss of income. Depending upon the impact on your home and family, you might have to spend a few days away from work. If you work from home, you stand to potentially lose your entire income during a power outage.
Having an automatic home backup power system like
A few essential precautions you should take in preparation for severe weather is to stock up on items, like food and water, and make necessary fixes, like boarding windows. Listen to a NOAA battery-operated weather radio for critical information from the
See more of these helpful tips from Today's Homeowner Danny Lipford: http://origin-qps.onstreammedia.com/origin/multivu_archive/PRNA/ENR/FX-Generac-092914.mp4. Visit the
About
Since 1959,
Photo - http://photos.prnewswire.com/prnh/20140304/CG76575LOGO
Video - http://origin-qps.onstreammedia.com/origin/multivu_archive/PRNA/ENR/FX-Generac-092914.mp4
SOURCE
Art Aiello, Public Relations Manager, 262-544-4811, x.2613, art.aiello@generac.com; Heather Gaedtke, Cramer-Krasselt, 414-227-3505, hgaedtke@c-k.com